1/16/2025 11:04 AM | |
Joined: 7/10/2024 Last visit: 8/22/2025 Posts: 180 Rating:
|
Hello IrontigerZ! If the program crashes when trying to enter the oB1, it may be indicative that there are corrupted temporary files that may have been corrupted. These temporary files are saved in the project's IM folder, so I recommend regenerating it. All files in this folder are recreated using a completely new build. The next FAQ "How do I delete the IM folder from the TIA Portal project?" may be helpful. I hope it works 🍀 |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
Follow us on