12/19/2024 12:20 PM | |
Joined: 12/2/2024 Last visit: 4/10/2025 Posts: 4 Rating:
|
Hello everyone. I'm starting the ebmpapst 5314/2TDHHP fan controlled by PWM. The fan datasheet: PWM input transistor requirements: UCEmax. => 12 V; I Sink max. > 5 mA; UCEsat. < 0,15 V Speed control:
By Puls width modulation (PWM) 0 ... 100% Open collector in relation to signal-ground. f: 2 kHz +-20% I used how-to-control-a-24v-valve-via-pwm-with-the-tm-pulse. I started it and it works, but the control range is only from 0 to about 20 (Output Value control - QW202), by ear this is its maximum speed. I set in TP Pulse. Operating mode: Pulse with modulation PWM, Parameter: Output format: Per 100 Minimum duration: 0 μs Period duration 500: μs. Manufacturer support said they have no experience with Siemens drivers. Maybe one of you guys knows how to set it up. --- Kristof |
12/19/2024 5:08 PM | |
Joined: 7/7/2010 Last visit: 9/12/2025 Posts: 16094 Rating:
|
Measure the PWM signal with an o-scope to see verify the following:
|
science guy |
|
12/20/2024 12:22 PM | |
Joined: 12/2/2024 Last visit: 4/10/2025 Posts: 4 Rating:
|
Unfortunately, there is no oscilloscope. ---- Kristof |
Follow us on