10/1/2024 2:36 AM | |
Joined: 8/20/2016 Last visit: 7/31/2025 Posts: 94 Rating:
|
I make a wincc flexible project but it not display "Transfer" function in the project colum like following picture. |
10/1/2024 6:45 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hello, Have you seen this link: How can you reset WinCC flexible to the original status of the last installation? Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
10/1/2024 6:53 AM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi phucxdtd, This is usually due to the internal configuration files of Flexible getting corrupted. You can try restarting WinCC Flexible. To do this, proceed as follows: 1. restart your PC (not absolutely necessary, but it is the safest option) 2. Once the PC has restarted, right-click on the WinCC Flexible Start Center in the Windows taskbar at the bottom right (see attached screenshot). 3. In the context menu, click on "Reset SIMATIC WinCC flexible" and wait until this process is completed. 4. Open WinCC Flexible again and check whether the loading icon is available again. Best regards!
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on