4/3/2018 9:01 AM | |
Joined: 10/25/2016 Last visit: 1/2/2023 Posts: 3 Rating: (0) |
Hi all, I am using a RFID system based in a RF180C communication module (ESIE6GT2002-0JD00) and two RF340R readers (ESIE6GT2801-2AB10). For manage this system I am using Ident Profile function blocks, "Ident_ResetRF300" (FB1920) and "Ident_Read" (FB1902). The problem that I have is sometimes, in function block "Ident_Read", BUSY bit is in state 1 and never goes to 0 and in a consequence of this DONE bit never goes to 1. To reset this anomaly I must download again instance data block of "Ident_Read" function block, clear bit EXECUTE of this function block and set bit EXECUTE of "Ident_ResetRF300" function block. In the attached file I share the part of the software code, also online, and the hardware configuration. PS: I already changed the RF340 reader, and RF180C for a new but the problem is still appearing. Thanks for all AttachmentAttach.zip (826 Downloads) |
Follow us on