5/31/2022 10:27 AM | |
Joined: 2/10/2015 Last visit: 5/21/2024 Posts: 96 Rating: (11) |
option_1 has to have the value 2 if you want to reset the LEDs with init after an error. If you're using RF310R Gen2 (6GT2801-1BA10) you can also set option_1 to value 3. Then the LED of the reader will be reseted after a successfull read or write command. |
Last edited by: AutoGen_242158 at: 05/31/2022 10:29:29 |
|
This contribution was helpful to1 thankful Users |
6/1/2022 5:15 AM | |
Joined: 5/16/2014 Last visit: 5/7/2024 Posts: 15 Rating: (0) |
I first try "option_1.bit 1" ,it not work. now it work now ,thanks |
Follow us on