(0)| 11/2/2018 12:28 PM | |
|
Posts: 4 Rating:
|
Hello sir, I am installed for TIA PORTAL V13 UP 6 BUT SIMATIC HMI KTP700 BASIC UPLOAD PROGRAM AT A TIME MASSAGE FOR ACTION CANCLED BEFORE UPLOADING DEVICE WHAT IS PROBLEM AND I AM UPLOAD FOR LAN WIRE ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/2/2018 5:14:20 PMNew subject after splitting |
|
| 11/5/2018 8:10 AM | |
|
Posts: 993 Rating:
|
Hello, what is the error message? can you post a screenshot?
|
| 11/14/2018 9:56 AM | |
|
Joined: 8/3/2009 Last visit: 12/4/2025 Posts: 16592 Rating:
|
Hello @ Hati that is not the Point in this case.... A Backtransfer is not possible in TIA Portal. --> Often the Words "upload" and "download"are used in the wrong context or people do not understand it without doubts. We should use the words "load to the Panel" and "loading from the Panel" then everyone knows what you mean. @ parmar ripal: check the Image Version of the Panel and compare with the Image Version in your Project. If its not equal then you have to do a OS Update first. In some Versions and situations the TIA Portal cannot do it automatically. in this case you have to do it manually first and then try to Load the Runtime Files to the Panel again. Here are some Basic FAQs: https://support.industry.siemens.com/cs/ww/en/view/58522603 https://support.industry.siemens.com/cs/ww/en/view/88633853 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on