(4)| 4/1/2008 1:50 AM | |
|
Joined: 1/20/2008 Last visit: 12/26/2025 Posts: 120 Rating:
|
FB99
Please download teh Attacment file. AttachmentINT_S5TIME.zip (6285 Downloads) |
Last edited by: MRG at: 4/1/2008 6:50 PM |
|
This contribution was helpful to
|
|
| 12/2/2013 10:37 PM | |
|
Posts: 2 Rating:
|
FC 40 WORKS FINE AND SMOOTH,,,, |
This contribution was helpful to
|
|
| 1/5/2014 1:05 PM | |
|
Posts: 1 Rating:
|
fc40 working fine |
| 11/22/2014 7:32 PM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Hello Milosh, Just to add some point in addition to what MicroMan has shared, The problem you are facing comes from the fact that SIMATIC timer has a section to automatically adjust the resolution.If you check the BCD output of timer, you can the last decade of the output to sse how it changes with the longer time spans.To get rid off all these problems, BCD output of Timer instruction is originally in S5TIME data type and can be easily converted to Time variable and more conveniently a value in seconds:
BCD Output of Timers-->FC33(from IEC library) -->Divide the result by L#1000 to have output in seconds. I hope this helps, Hamid Hosseini Attachmenttest.zip (1400 Downloads) |
This contribution was helpful to
|
|
| 11/23/2014 10:04 AM | |
|
Joined: 8/16/2010 Last visit: 1/17/2026 Posts: 640 Rating:
|
Nice. Thank you... |
This contribution was helpful to
|
|
Follow us on