(0)| 8/1/2006 2:34 PM | |
|
Posts: 317 Rating:
|
Hi, I don't think this can be done like you want. It's easy to create a recipe on TP1 and see the values on TP2. Just use the plc as a gateway and use PLC jobs to update the recipe values on TP2. The problem I can see is there is no way to build a list of recipe names on TP2 after they are created on TP1. Unless someone else has a different idea? It's maybe of no use to you but if the TP was TP177PN/DP then you could create the recipe on TP1 and use Sm@rtaccess to select the recipe on TP2. |
Last edited by: skimmer at: 8/1/2006 2:35 PM |
|
| 8/1/2006 4:32 PM | |
|
Posts: 3149 Rating:
|
Hi, perhaps this FAQ can help? http://support.automation.siemens.com/WW/view/en/22777466 nemo |
| 7/13/2015 1:15 PM | |
|
Posts: 4757 Rating:
|
|
Follow us on