1/31/2011 11:36 AM | |
Posts: 79 Rating:
|
how will update cp342-5 v5.7 in hardware catalog step 7. Splitted from i cannot find firmware cp 342-5 version v5.2 on the internet help?. |
Last edited by: O_Moderator at: 1/31/2011 12:31 PMnew subject after splitting |
|
1/31/2011 12:00 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, The firmware can be updated via a download of the firmware. You will find the firmware update V5.7 for the CP 342-5 / CP 342-5 FO (order no.’s 6GK7342-5DA02-0XE0 / 6GK7342-5DF00-0XE0) under entry ID: 24105718. In STEP7 you should continue to configure the module as V5.0. BTW newer version of CP was released. Look at 6GK7342-5DA03-0XE0 with firmware 6.0. Best regards, Hristo Mihalev |
1/31/2011 12:33 PM | |
Posts: 79 Rating:
|
please try to understand i got and downloaded how will updtate my catalog in step 7 |
1/31/2011 12:37 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Please read it carefully.
Best regards, Hristo Mihalev |
1/31/2011 12:42 PM | |
Posts: 79 Rating:
|
i configured but still in stop mode . module version error is coming |
2/1/2011 5:17 AM | |
Posts: 79 Rating:
|
I ATTACHED SCREENSHOT FOR GETTING ONLINE ERROR MESSAGE.
Attachmentuntitled.pdf (448 Downloads) |
2/1/2011 6:43 AM | |
Joined: 10/7/2005 Last visit: 9/4/2025 Posts: 3049 Rating:
|
Hello boopathi@sequent Your 315 can't "see" the CP and three possible reasons for thisproblem come to mind: 1.) Check your CPU part numberand firmware and see if it is in the listof the following FAQ (it is is, follow its remedy advise): What do you have to do if the SIMATIC S7-300 CPU no longer goes into RUN mode after adding a CP or FM module? 2.) If the above is not applicable, verify that you have 24DC conencted to the CP342-5 3.) If you have, verify that the U shaped backplane connector is inserted between the CPU and the CP. That's all I can think of andI hope this helps |
Cheers |
|
Follow us on