(1)| 5/13/2014 5:59 AM | |
|
Joined: 5/28/2008 Last visit: 1/3/2026 Posts: 4522 Rating:
|
Hello, Force function is made to change the physicalstatus of inputs (for instance) and let the CPU execute the program with this forced input. For example, if you forced a DI to be high, while this DI is physically low, the CPU will execute the program as if this DI is high. Force orange led of the CPU will lit when you force any variable.
If you are working offline, you do no need force table. All what you need to simulate your program is to open Input windows in the PLCSIM and check mark the inputs you would like to simulate On. All necessary info can be found in this manual:S7-PLCSIM And please read these important FAQs. Hope this helps.
|
|
Ayman Elotaify |
|
This contribution was helpful to
|
|
| 4/11/2018 2:52 PM | |
|
Posts: 8171 Rating:
|
New question published by Basketballer is split to a separate thread with the subject Is it possible to force states just after changing mode into STOP?. Best regards |
Follow us on