(3)| 10/31/2008 6:12 AM | |
|
Joined: 10/7/2005 Last visit: 1/14/2026 Posts: 3054 Rating:
|
Dear Rawat SFC13 is dedicated to read out Diagnostic information from a DP Slave (no more and no less). SFC51 on the other hand reads out the S7 system status list. When you call SFC51 you decide via the "SSL-ID" Block input in combination with the "Index" block inout what part of the S7 system status list you want to read (e.g. the status of the LED's on the CPU, serial number of the memory card, assignment of all process image partitions to OBsetc. etc. etc. etc.). Use the online help (F1) on SFC51 to find out how powerful and usefulSFC 51 really is (I am abig fan of it) If you call SFC51 with and SSL-ID of W#16#00B4 andthe DP Slave Diagnostic address as the Index, then (and only then)does SFC51 has thesame funtionality as SFC13. I hope this helps and clarifies things. |
Last edited by: fritz at: 11/1/2008 11:54 AMHello again Rawat I just realised that I did not read your question properly. The short answer would have been that they deliver the same result in this case, SFC13 does however has a faster execution time (see Instruction List manual for more). Cheers |
|
This contribution was helpful to
|
|
Follow us on