(2)| 6/12/2009 7:46 AM | |
|
Joined: 1/29/2006 Last visit: 12/16/2025 Posts: 451 Rating:
|
Hey, Chiara! Do you have to save your "list of fixed ingredients" and use it again next time (with the same quantities)? If so, then you are dealing with recipe handling and option UserArchive is a proper tool for you. This option provides a complete support for recipe handling allready in basic use, you only have to configure your archive (in Wincc Explorer) and then add a User archive table in your pdl. This table provides you with all of the needed functionality for work with recipes. See, what WinCC help system says about that. The only manual, that I have found on net for UA, is at the following link: http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&objid=10805594&treeLang=en This is a Manual for WinCC options, Ver6, and there is a good chapter about User Archives. It includes also an example of Scripting, if the basic functionality is not enough for your application. Have fun! uel123 |
| 6/12/2009 10:58 AM | |
|
Posts: 18 Rating:
|
Hi uel123, Now I'm trying with control variables... Thanks for suggest, I moved the discussion to Wincc section. kindly regards |
| 6/15/2009 8:26 AM | |
|
Joined: 9/1/2005 Last visit: 10/31/2025 Posts: 4114 Rating:
|
Thread is closed because the question is posted twice. You will find this question with the subject User Archives VS Tag logging within the conference SIMATIC WinCC Best regards CS Moderator |
|
My Forum is the place to personalize your profile, |
|
Follow us on