(1)| 6/20/2010 6:58 AM | |
|
Posts: 36 Rating:
|
Are using serial com port in your PC or USB converter to serial? It seem as like my problem when using USB converter or third party S5 USB cable. |
| 6/20/2010 7:41 AM | |
|
Posts: 68 Rating:
|
Dear Pedro Ascencio, Hi I am also fased same problem in serial S5 communication .Hear I have attached the manual,may Attachment5 Simple Steps to Configure Serial to USB conversion on St….pdf (712 Downloads) |
Last edited by: S5 SHOOTER at: 6/20/2010 7:42 AM |
|
This contribution was helpful to
|
|
| 6/21/2010 9:46 PM | |
|
Posts: 56 Rating:
|
Thank you for your help, but I have a different connection, not via USB. My link is between ethernet port (PC) to serial port (SI1, PLC-S5) via S5-PCLink Software-Converter. The software creates a virtual serial port so that you can select this port in "parameter setting" of the STEP 5 software. The converter is put on SI1 (it has an ethernet ip address), so that you can access to PLC likes ethernet link. My problem occurs downloading big PBs. In this case appears "time out". The solution was not only modifying the Baud in "S5@@@@AS.INI", but was necessary increase "Block_Time" parameter. Well, now we do not have any more problems, but I would like to know what does each parameter means?, or what do modifications Siemens recommend ? to avoid problems like these. Best regards. Pedro |
Follow us on