(1)| 6/15/2010 6:39 PM | |
|
Joined: 3/21/2006 Last visit: 10/16/2025 Posts: 10239 Rating:
|
Hello, You can use the following RS232/PPI Multi Master cables for downloading a project: Order Number: 6ES7901-3CB30-0XA0 The RS232/PPI Multi Master cable (with 8 DIP switches) can be used if DIP switch number 5 is set to PPI/freeport ("0"). The cable must be dead for it to accept the change. Look at How do you backup/restore with a Windows-based panel? (baud rate best regards, Hristo Mihalev |
| 6/16/2010 8:36 AM | |
|
Posts: 719 Rating:
|
Don't try to execute OS Update before uploading a backup, because it will erase the HMI software downloaded on the panel. |
| 6/19/2010 11:23 PM | |
|
Joined: 5/28/2008 Last visit: 12/23/2025 Posts: 4522 Rating:
|
Hello Simon Wales, No, It's not possible to lock the HMI in order to disable backup function. I think that the problem is in the connection. Please have a look on this FAQ to chose the suitable transfer option to you What transfer options are available in the various operator panels? Regards. |
|
Ayman Elotaify |
|
Follow us on