(0)| 10/6/2010 3:38 PM | |
|
Posts: 45 Rating:
|
Dear Experts, I am going to develop a SCADA system by means of PCS7 Telecontrol. There are about 45 substations which should be controlled by SCADA via IEC870-5-101. Each substation contains about 250 tags to be monitored. Please help me to know: 1- If development of such SCADA system is possible 2- What do i need for system network switcher. I mean the switch which receives data from 45 substations and delivers two redundant nodes to be connected to SCADA's Redundant Ethernet and manages them. A network architecture of the system which is going to be developed is attached. Splitted from Scada data gateway- ICE 60870. |
Last edited by: O_Moderator at: 10/8/2010 8:14 AMnew subject after splitting Last edited by: rezajan55 at: 10/6/2010 3:51 PM |
|
Follow us on