(0)| 10/20/2010 8:00 PM | |
|
Posts: 156 Rating:
|
1. An S5 95U 8ME DP Master with procibus slaves 95U 8MD DP Slave and OP15 I was programming online a simple rule in an PB In de u DP Master I programmed : L MB107 L KF+1 !=F = M105.0 When i saved it ,STEP5 said the memory is full, Compressing? i said yes after compressing the PLC whent to stop???? Maybe because of the EEPROM IS both for S5 and Profibus parameters BF Led is ON STOP Led is ON After After some trying , PLC Stop run /Voltage switch of PLC OFF/ON WE DID NOT PRESS COPPY because we think it wil loose the profibus data Master CPU BF Led was not on And master CPU run led is ON Slave CPU BF Led was ON and RUN is on But if BF master led is not on /and slave BF led is on we think Profibus parameters ar allreade lost We reloaded the Profibus parameters in the PLC and after this the S5 Program(when transfering it asked 3 times to compress) After this we got the CPU and the Profibus running again We try to program the the code again L MB107 L KF+1 !=F = M105.0 Now it did not asked to compress en the code works perfect Weard? Second questions was splitted to problem With an 95U 8MD DP Slave. |
Last edited by: O_Moderator at: 10/21/2010 8:43 AM |
|
Follow us on