(0)| 10/20/2010 8:00 PM | |
|
Posts: 156 Rating:
|
problem With an 95U 8MD DP Slave We made an FB50 With 3 Declarations PULS E BI COUN A W REST E BI ON E BI And Some Code We call the fb 4 times with diffrent parameters If we look at the block online we can't see the status of the parameters of the block And step 5 says something like Netwerk nicht bearbeitet when the cursor is on the block But When i look at the variables online I see the block works perfect The code in the block is -------------------------------- PULS E BI COUN A W REST E BI ON E BI UN =ON If counter is on go futher SPB =M001 UN =PULS if countpuls add 1 SPB =M001 L =COUN load count word L KF+1 load 1 +F add 1 T =COUN transfer count word M001: UN =REST if reset load 0 transfer count word SPB =END L KF+0 T =COUN END: BE ------------------------------- Splitted from S5 95U 8ME DP Master with profibus slaves 95U 8MD DP Slave and OP15. |
Last edited by: O_Moderator at: 10/21/2010 8:47 AMnew subject after splitting |
|
| 10/21/2010 2:54 PM | |
|
Posts: 156 Rating:
|
totday i tested just the same block in an S5 944 115U CPU and in this plc it shows the variables But in the 95U it does not. |
Follow us on