3/15/2011 7:21 AM | |
Posts: 32 Rating: (0) |
Hi I have some questions realted to winCC and i hope experts here will to get all my confusions cleared. Archive files are always stored so that they are local to the computer in the associated project. [schnippschnapp] other questions can be found in the following threads What is the difference between fast archiving and slow archiving. |
Last edited by: O_Moderator at: 3/15/2011 11:25 AMnew subject after splitting |
|
3/16/2011 10:49 AM | |
Posts: 1530 Rating: (59)
|
Hello panthripu, yes, you can copy your files to another place, but take care that the order stays the same, because otherwise you will have problems with retrieving it. If you want to retrieve them, you have to add the symbol "connect backup" and "disconnect backup" to your toolbar, you will be asked for the location of the file, if you select "connect backup" in runtime. There is also a helpful FAQ. Includes a WinCC PDL-File, with which connecting oder disconneting of archives will become a little bit more comfortable. Best regards Bizur |
Follow us on