(0)| 5/17/2011 7:12 PM | |
|
Posts: 11 Rating:
|
Hi Sarabjot, Are you using TIA Portal V11 for your PLC? If so, you can use the Data Logging feature to write a CSV file with the tag values you want to keep track of. I have posted an example program with a FB to set up and maintain a data log here. You may need to modify it for your application, but it would be a good starting point. Again, only really useful in this case if you are already using TIA Portal V11, but should be an easy solution if you are. Best Regards |
| 5/17/2011 7:33 PM | |
|
Joined: 3/21/2006 Last visit: 10/16/2025 Posts: 10239 Rating:
|
How can WinCC exchange data with Microsoft Excel or Access? Best regards, Hristo Mihalev |
| 5/20/2011 10:03 AM | |
|
Joined: 2/6/2009 Last visit: 11/7/2025 Posts: 46 Rating:
|
Here is simple example of VBS script for writing tag values in csv file from WinCC. Best regards, VladD AttachmentWinCC_VBS_WriteTagInFile.zip (3977 Downloads) |
This contribution was helpful to
|
|
| 5/20/2011 1:53 PM | |
|
Posts: 166 Rating:
|
Dear ABN , Suppose , If those tags, I dont want to use in Trends , just only want to export it to Excel , Will it work? Thanks. Your's Truly, Sarabjot Singh Manku |
| 5/20/2011 2:08 PM | |
|
Joined: 10/3/2010 Last visit: 12/18/2025 Posts: 1571 Rating:
|
did you read the other replies above? Seems already an answer to your question in there |
|
B r g d s , |
|
| 5/30/2011 5:40 AM | |
|
Posts: 212 Rating:
|
Dear |
Follow us on