(0)| 5/25/2011 5:44 AM | |
|
Posts: 96 Rating:
|
Dear all, I have a project using S120 CU310-DP (serial 6SL3040-0LA00-0AA1) and servo motor 1FT7082-1AF71-1DH1. My servo package hasn't arrived so I don't have compact memory to use GSD file in it. I've downloaded GSD file of Sinamic S120 on this forum. I download 2 file: SI0380E5.GSE and SI2580E5.GSE. I use Sycon software to config communication from Schneider PLC and S120 and have some questions: 1. I want to control speed and position which setpoint is sent from PLC, so in Starter v4.2 I choose Telegram 9 to use MDI Mode. I look in GSD file SI0380E5.GSE have the correct serial of my CU: "MLFB: 6SL3040-0xA00-0xxx", but it doesn't has Telegram 9. In file SI2580E5.GSE I don't see information about serial of CU310-DP, but it has Telegram 9. Can I choose GSD file SI2580E5.GSE? Or if I choose file SI0380E5.GSE, can I use Telegram 9? [schnippschnapp] second question can be foun in the following thread When using MDI Mode, Can I change speed and possition from PLC when motor is running?. |
Last edited by: O_Moderator at: 5/25/2011 8:21 AM |
|
| 5/25/2011 7:40 AM | |
|
Joined: 3/21/2006 Last visit: 10/16/2025 Posts: 10239 Rating:
|
Hello, The correct one is SI2580e5.zip. (depends of real firmware version of CU.) Best regards, Hristo Mihalev |
| 5/26/2011 1:06 PM | |
|
Joined: 3/21/2006 Last visit: 10/16/2025 Posts: 10239 Rating:
|
Hello, Means firmware of the CU. http://support.automation.siemens.com/WW/view/en/49216293 You will need card reader which supports CF card. This is a normal card reader (7 in 1, 12 in 1...). And just copy the file from directory /SIEMENS/SINAMICS/DATA/CFG. Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 5/26/2011 1:12 PM1. What is difference between SIMATIC S and SIMATIC S DXB? Is this means SINAMICS S and SINAMICS S DXB? Last edited by: UMENCHO at: 5/26/2011 1:09 PM |
|
| 5/26/2011 5:08 PM | |
|
Posts: 96 Rating:
|
Hi UMENCHO, Thank you for your answer. I have a mistake in my first question. I mean What difference between SINAMIC S and SINAMIC S DXB. |
Follow us on