(0)| 5/25/2011 5:44 AM | |
|
Posts: 96 Rating:
|
Dear all, I have a project using S120 CU310-DP (serial 6SL3040-0LA00-0AA1) and servo motor 1FT7082-1AF71-1DH1. My servo package hasn't arrived so I don't have compact memory to use GSD file in it. I've downloaded GSD file of Sinamic S120 on this forum. I download 2 file: SI0380E5.GSE and SI2580E5.GSE. I use Sycon software to config communication from Schneider PLC and S120 and have some questions: [schnippschnap] 2. When using MDI Mode, Can I change speed and possition from PLC when motor is running? Or I must stop motor and apply the change, then sent command to start it again? Splitted from Using Telegram 9 in CU310-DP with motor 1FT7. |
Last edited by: O_Moderator at: 5/25/2011 8:20 AMnew subject after splitting |
|
| 5/29/2011 3:53 PM | |
|
Posts: 96 Rating:
|
Thanks for your answer, IBN-Service. I get it. Best regards. |
| 5/29/2011 4:28 PM | |
|
Posts: 8946 Rating:
|
You are welcome! |
| 5/30/2011 3:16 AM | |||
|
Posts: 96 Rating:
|
Hi UMENCHO, I downloaded file SI2580e5.zip. It's include some file which the same name but different extention: SI2580e5.GSE, SI2580e5.GSI, SI2580e5.GSG, SI2580e5.GSS, but I can't see file SI2580e5.GSD, so I choose SI2580e5.GSE for English. I have following your link at http://support.automation.siemens.com/WW/view/en/49216293 and downloaded file SI2280E5.Zip coresponding to my CU firmware is v2.6. Today (30-5 in my local time), our package is arrived. I will test it and give you result. I hope it work. Please help me in topic
Regards. |
||
Last edited by: chicken at: 5/30/2011 6:39 AM |
|||
Follow us on