12/1/2015 10:19 AM | |
Joined: 8/25/2014 Last visit: 7/2/2024 Posts: 166 Rating: (2) |
Dear MAZENJER,This is very helpful information. Can you please help me more how I can configure the status word and control word inside the drive. Measn how can I link it inside the drive. And How can we transfer the digital output bit status of drive to plc?
|
12/1/2015 10:51 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello Kshf, If you use STEP7 "classic" go to Hardware configuration, to the right on the tree select PROFIBUS, then SIMOVERT, MICROMASTER 4 click MICROMASTER 440---> 6SE6400-1PB00-0AA0 with drag and drop put in the Profibus network Also please have a look: MICROMASTER/SINAMICS G: Speed control of a G120/G120D/MM4 using a S7-300/400 (STEP 7 V5) with PROFINET/PROFIBUS and HMI |
This contribution was helpful to1 thankful Users |
12/3/2015 10:34 AM | |
Joined: 8/25/2014 Last visit: 7/2/2024 Posts: 166 Rating: (2) |
Dear Ste39, Thanks a lot for useful information. I need actually the same information which you attached here. |
12/3/2015 10:43 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Dear Kshf, in the link above there are also examples, or if you're looking in the forum there are many threads that explain how to do: (Read from) / (Write to) MICROMASTER 420 from STEP 7 ...Accessing Micromaster 440 Parameters on S7 PLC - Entries ...use profibus and step 7 manager to read/write mm440 ...MM4 and S7-300 on PROFIBUS read / write values - Entries ... |
Follow us on