3/5/2015 11:35 AM | |
Posts: 2 Rating: (0) |
Hi all, I'm trying to get a connection between a PC station and my PLC (S7-1500). I'm using TIA Portal V13 and Siemens Simatic NET V12. I can see my connection in OPC Scout V10 but when i'm trying to open a data block, this object is empty. Further I can see at "OPC.SimaticNET" at status the following: "The server is running normalliy". And in my software in TIA Portal V13 I have the following (see attachment) Can someone please help me? Thanks in advance.
|
Last edited by: Min_Moderator at: 3/5/2015 2:29:46 PMNew subject after splitting |
|
11/2/2015 4:56 PM | |
Posts: 439 Rating: (109) |
Gaël, You just need to know where to find information, Siemens website is huge. Siemens technical support is awesome and save me so much time. Please see attach file, it is a procedure to connect an OPC server with S7-1200 and it is relatively the same with S7-1500. There is also Youtube video about this. You can also find lots of information into the manual of SIMATIC Net V12. Best regards, Hugo Attachment39960679_S7-1200_OPC_SIMATIC-NET_TIA-Portal_e.pdf (1749 Downloads) |
Follow us on