2/16/2016 1:25 PM | |
Joined: 3/14/2008 Last visit: 8/7/2024 Posts: 2080 Rating: (931) |
muneeb, The master library is to make sure that you use blocks that are designed for your project. When you insert new blocks, you need to grab them from the master library. If you need to update a block, you will do that first in the master library and then distribute them over your project. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on