6/1/2016 1:20 PM | |
Joined: 8/16/2015 Last visit: 6/6/2022 Posts: 37 Rating: (0) |
Dear All, Kindly we need your help , We made the configuration for CP341 As attached but we found the led TX flashing but RX led do nothing , and no data from the slave device collected ,we put FB10 on OB1& FB35 at OB35, In online mode we found Status=16#0,Done=0 ,error=0 the wiring diagram is B+ of master to B+ at slave & A+ of master to A+ at slave Regards, Saleh Hany ------------------------------------------------------------------------------------------ AttachmentCommpdf.pdf (291 Downloads) |
Last edited by: Min_Moderator at: 6/2/2016 11:59:13 AMNew subject after splitting |
|
6/1/2016 11:03 PM | |
Joined: 8/16/2015 Last visit: 6/6/2022 Posts: 37 Rating: (0) |
Dear TIBI68, Our type of Communication Processor is CP341 ( 6ES7-341-1CH02-0AE0 ) also Kindly find the attached file of the Slave device configuration & wiring ( Elster FC 2000 flow computer ) (the wiring diagram at page 96) , we made the connection with two wired configuration pin 6 (FC side) to pin 11 (CP side) & 9 (FC side) to pin 4 (CP side) Regards, Saleh Hany AttachmentFC200 config&wiring.zip (209 Downloads) |
6/3/2016 1:55 AM | |
Joined: 8/16/2015 Last visit: 6/6/2022 Posts: 37 Rating: (0) |
Dear TIBI68, Thanks for your support, Kindly find the attached file of FC 2000 wiring and FC RS485 configuration (sorry for the empty attached) Now we leaved the site and we will return at the next week, to complete our work and we will check the DB 303 ( as our configuration) , we thought that the data will be at DB 305 ( as our configuration that assigned for S7ADDR parameter of FB10) but now you told us that the data will be at DB 303 , Also Mr TIBI68 we need to make sure that Done=0 Error =0 status=16#0 is this values ok ( healthy ) ? again we want to thank you very much for your appreciated help ,and we will give you the feedback immediately after check data on DB303 Regards, Saleh Hany AttachmentFC200 config&wiring.zip (217 Downloads) |
Last edited by: Saleh_1 at: 6/3/2016 1:59:54 AMLast edited by: Saleh_1 at: 6/3/2016 2:44:37 AMLast edited by: Saleh_1 at: 6/3/2016 2:54:11 PM |
|
6/6/2016 1:44 PM | |
Joined: 8/16/2015 Last visit: 6/6/2022 Posts: 37 Rating: (0) |
Dear Mr TIBI68, I was at site yesterday and i had some image as attached and also had video for the changeable data at DB 303 ( changeable only when we connect the cable between CP & Salve device and CP led TX& RX blinking ), we made a configuration for a minor data request from the slave device but also didn't find the data at S7ADDR data block or also at DB303 ,Please we need your help The video link is (https://drive.google.com/open?id=0B2--eAyZ6SzRUUY0ZlYyb0pOREk) Regards, Saleh AttachmentCP-341 serial_config( 1 ).zip (250 Downloads) |
Follow us on