12/3/2019 11:52 AM | |
Joined: 12/14/2011 Last visit: 5/3/2024 Posts: 166 Rating: (14) |
Hi to all, TIA V16 is available for the download. The trial software can be download here: https://support.industry.siemens.com/cs/ww/en/view/109771626 Good job. |
Last edited by: gigi_plc at: 12/03/2019 12:23:20Last edited by: gigi_plc at: 12/04/2019 15:55:50Last edited by: gigi_plc at: 12/05/2019 14:34:24 |
|
This contribution was helpful to9 thankful Users |
12/10/2019 3:54 PM | |
Joined: 12/14/2011 Last visit: 5/3/2024 Posts: 166 Rating: (14) |
S120 CU310 now is available.. |
1/28/2020 1:39 PM | |
Joined: 12/14/2011 Last visit: 5/3/2024 Posts: 166 Rating: (14) |
Yes, you are right.. i had several times TIA V16 crash.. update 1 is required as soon as possible.
|
2/26/2020 5:57 PM | |
Joined: 11/7/2019 Last visit: 7/7/2021 Posts: 1 Rating: (0) |
Has this bug been fixed yet? Determining if I should start a project on V16 or V15. Thanks! |
Follow us on