11/15/2010 3:07 PM | |
Joined: 9/27/2006 Last visit: 8/4/2024 Posts: 12273 Rating:
|
Hello Richard; Profinet uses a TCP/IP physical layer and data transmoission layers; as such, many protocols can cohabitate on the network without problems, as long as collisions do not interfere with transmissions (Profinet is immune, not Modbus/TCP). If you care to check, you can search the forum on the subject, you will see that the question has been asked a few times before, and that the consensus is that you can go ahead.One example: PROFINET TCP/IP and Modbus TCP/IP Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/15/2010 3:08 PM |
|
11/15/2010 3:16 PM | |
Joined: 1/17/2007 Last visit: 7/29/2024 Posts: 1544 Rating:
|
You do not need any additonal hardware. You can use the PN port of the CPU for modbus TCP. You will need some additional software from IT4Industry. See this post. |
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
7/21/2015 10:31 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
|
Follow us on