9/5/2013 4:05 AM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Hello Juan; A gsd file is only used to integrate a Profibus-DP slave from a (non-Siemens) vendor into a Step 7 configuration package, it would not help you in the present case. Maybe the following Update information for your CPU model can clear up the issue: Delivery Release for Innovated SIMATIC S7-1200 with Firmware Version 3.0 TheSIMATICS7-1200 with firmware version 3.0 and higher can be programmed with STEP7 Basic V11 SP2 Update3 or higher. Programming theS7-1200 with FW 3.0 and higher with older STEP 7 versions or with STEP 7 Micro/WIN is not possible. See here for the download links for update 5 of SP2, Step 7 Basic V.11: |
10/10/2013 9:17 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715) |
Hello, It's easyer to search on partnumber i.e. 6ES7 223-1PL32-0XB0. Then in the entries select download, that leads you in no time to the HSP's Step-7 v11 HSP Regards, Marcjan |
Problem solved? |
|
2/25/2016 1:19 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by zapla1 is split to a separate thread with the subject Upload doesn't work. Best regards |
Follow us on