11/27/2015 2:14 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hello, the interfaces ar desribed in the S110 manual capter 7.3 https://support.industry.siemens.com/cs/ww/en/view/109478122 what do you mean whith the adresses? Whit this adresses you can communicate with the S110. To configure the S110 that it use the correct signals from the fieldbus you should use starter.
Christoph |
11/30/2015 12:09 PM | |
Joined: 7/7/2015 Last visit: 9/4/2023 Posts: 55 Rating: (0) |
Thank you. Address.. in photos, 'I0.0' is my inputmodule address. but, I don't know what is assigned on coil. Q 280...283? But How I know function of 280...283? I configured on H/W configure, But, In STARTER, there are some problems... I guess, Online assess point is S7ONLINE(STEP7) PG/PC interface is PC Adapter(MPI) anything wrong...? I communicate PLC with MPI - ET200M with ethernet - S110 with ethernet. Attachmentphoto.zip (179 Downloads) |
Last edited by: Ssung at: 11/30/2015 12:10:10 PM |
|
11/30/2015 3:49 PM | |
Joined: 7/7/2015 Last visit: 9/4/2023 Posts: 55 Rating: (0) |
Thank you.. I have 2 Questions. 1. In photo, there is circuit. In starter, I set S7ONLINE, PG/PC interface: PC Adapter[Auto], Target address: CU305 Here, PG/PC interface have to be MPI? Or TCT/IP? OR Auto? Target address have to be CU305's address? When I connect ethernet direct CU305, DeviceMode, Online Node finds CPU&ET200M, theose are unable to connect... 2. When I Configue In STARER, Can I map address on communication parameter? In list, Module contents apperears? Sorry.. AttachmentNew Folder.zip (197 Downloads) |
12/1/2015 3:15 PM | |
Joined: 7/7/2015 Last visit: 9/4/2023 Posts: 55 Rating: (0) |
By your advice, I Solve problem 1). Thank you. Know I communicate with CU305 by PLC. But... problem 2) makes me hard. Is 'Slots of the Drive Object' located in H/W configure? And, I tried activate motor using DO"Drive_1, It didn't active... Here are photos. I makes i 2.0- Q280.0 ...i2.7-Q280.7 My act is wrong? And I don't know what STW means. Attachmentphotos.zip (175 Downloads) |
Last edited by: Ssung at: 12/1/2015 3:18:03 PM |
|
12/1/2015 3:29 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hi, STW means Control word. With the Control word you give the signals from the PLC to the drive and then the drive state machine interact with this control word signals and activate the motor. The shematic of the state machine is described in the List Manual and Function manual . Regards Christoph |
12/15/2015 2:34 PM | |
Joined: 7/7/2015 Last visit: 9/4/2023 Posts: 55 Rating: (0) |
Hi~ I get sample motor program. But there are some quastions. 1. In I/O address, what should i set address? Drive_1(Motor) Or Control_Unit(Inverter)? I Think Drive_1, But I Don't Know why.... 2. There are fatal error, Is this error occured because of "#Read Inveter?" In SFC 14, I think "#Read Inveter" should be "312". But it is "0'.... 3. In Question 2, SFC14 if correct system function? This program was 315-2DP's Program. I changerd CPU,315-2F PN/DP. Thanks! AttachmentPhoto1.zip (182 Downloads) |
Follow us on