1/11/2012 1:47 PM | |
Joined: 12/11/2009 Last visit: 9/8/2022 Posts: 243 Rating: (4) |
Hello I have following error (in attachment) I tried to change user rights but nothing changed. can u help please I tried these /tf/WW/en/Posts/14795 https://support.automation.siemens.com/WW/llisapi.dll?func=ll&objid=22679730&nodeid0=10805600&caller=view&lang=en&siteid=cseus&aktprim=0&objaction=csopen&extranet=standard&viewreg=WW |
1/12/2012 4:39 PM | |
Posts: 1530 Rating: (59)
|
Hello Osman_, I think there is a missunderstanding in using the thread from forum and FAQ: "How can you avoid the "DEMO mode" of the WinCC Web Navigator client? You have to remove the marks for function 1002, because this in reserved for data monitor. But I must admit that FAQ shows only screenshots including this mark, so this can cause missunderstandings. Maybe someone (either you or me) write a "Suggestion for this entry" - maybe describtion will be improved than. Best regards Bizur |
1/13/2012 12:32 PM | |
Posts: 1530 Rating: (59)
|
Hello Osman_ I've just found something which could be also of interest for you: Which operating system and software do you require for the SIMATIC WinCC Web Navigator V1.x, V6.x and V7.x? I know it contains lots of information, but who knows ... Best regards Bizur |
3/28/2012 6:23 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating: (71) |
Hi autobots, check the file C:\Program Files\Siemens\WinCC\diagnose\LicenseLog.xml for errors. Also helpful: http://support.automation.siemens.com/WW/view/en/38645769 http://support.automation.siemens.com/WW/view/en/44029135 http://support.automation.siemens.com/WW/view/en/23173286 http://support.automation.siemens.com/WW/view/en/23322349 |
mfG / Best regards |
|
11/24/2012 9:35 PM | |
Posts: 10 Rating: (1) |
One possible cause for this error is trying to run user archive without an license to it. |
Follow us on