Industry Online Support
Technical Forum
7/26/2013 10:03 AM | |
Joined: 8/10/2009 Last visit: 4/25/2024 Posts: 166 Rating: (2) |
PLEASE REFER THIS THREAD IN REFERENCE TO MY THREAD : /tf/WW/en/Posts/95469#top ------------------------------------------------------------------------------------------------------------------------------------ Dear Enia /Mr. Pegaia , That means , there are more people facing the same issues . I found out one thing in relation to it ( FROM MY POINT OF SCENARIO) : The Machine on which , The code is working is an fresh newly installed system with all the Siemens Softwares like Simatic TIA PORTAL V11 , Simatic Wincc TIA PORTAL V11 . And the Machine on which Its not working is : having the same Windows and Same software , The only Difference is : It is running inside a VMWARE , version 3 build 203739 Then I tried one tricky thing , I made the image of that system in which The code is running well in Simatic TIA V11 and installed the same on a seperate system . You know surprisingly what came out : The instruction which was working in original PC was not working in this sytem . Conclusion ( As per Me) : VMWARE doesn't support all the Scada functions for Siemens ( For Other Scada's need to explore ) If any body want to add anything , please go ahead . Waiting for your valuable Comments . Thanks. Sarabjot Singh Manku |
Follow us on