4/26/2016 12:02 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hi Tomact, Which font is used for the tooltip text? Default it should be "Arial". If the font looks correct, maybe you can change it back and forth, save the screen and see in runtime the result. |
If I could help you, you can use the RATE button. Thank you. |
|
4/26/2016 12:24 PM | |
Posts: 75 Rating: (18) |
Hello Tomact, in case it's possible for you to update to WinCC V7.3 Update5 I've good news for you: Your found problem seems to be solved with Update5. You have to install the update and then to rerun the migration from WinCC V7.0 SP2 Update8. Hope this solves your Problem. Regards, |
This contribution was helpful to1 thankful Users |
Follow us on