Industry Online Support
Technical Forum
10/26/2014 3:47 PM | |
Posts: 5 Rating: (1) |
hi hello, i have problem with sinamics G120 CU240B-2DP drives warning alarm is coming A30016 (power unit: load supply switched out(23)) this alarm is displaying in the starter software because of this alarm drive ready condition is not enabling after manual reset from the panel the drive ready condition DO is not energising , after this DO energising from drive condition only Auxillary contact will pick up and given signal to the power unit then i can start the motor . if i upload other drive parameter data to PG and then download to this drive(target device) through online still the the problem exist , so kindly give me the precaution(remedy) for this issues as soon as possible waiting for the reply.
---------------------------------------- New subject after splitting from Problem With Sinamcis G120 + CU240B-2DP |
Last edited by: Min_Moderator at: 10/27/2014 1:24 PMSplitted Thread Last edited by: Min_Moderator at: 10/27/2014 1:24 PMSplitted Thread |
|
6/16/2016 3:25 PM | |
Posts: 2 Rating: (0) |
I have exactly the same problem... Did you solve this issue? If yes, can you tell me how to solve it? Thanks in advance! |
6/17/2016 10:46 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please check the alarm value in r2124. |
Follow us on