Industry Online Support
Technical Forum
11/28/2014 5:36 AM | |
Posts: 17 Rating: (0) |
Dear Expert, I 'm now working with data loging , i have some question as below : 1. Datalog Create : In my step 7 ( tia portal v13.0) data log create dont have the "HEADER" parameter. My cpu is 1214c firmware 3.0. Please see the attached file. 2.Datalog new File : How many datalog New file can PLC save and display in webserver if the Memory card is 4MB. and if the datais full, the new DatalognewFile will overwrite the oldest one ? If i want to delete the datalognewfile , only in webserver can delete it ? In plc have any function to delete this file ? Thank in advanced .
AttachmentData-Log Create.pdf (1037 Downloads) |
11/28/2014 3:43 PM | |
Posts: 267 Rating: (22) |
Hello Tony, 1. the parameter "HEADER" is hidden. It will be displayed when you click on the arrow in the buttom of the block. 2. chapter "Calculating the size of a data log file" (page 394) in http://support.automation.siemens.com/WW/view/en/91696622 Yes, you can delete the csv-file in the webserver only. Do you know this application? http://support.automation.siemens.com/WW/view/en/64396156 |
12/1/2014 11:37 AM | |
Posts: 267 Rating: (22) |
Hi Tony, "DataLogCreate.Status" = 16#7000 means "No job processing active." You must set the bit "DataLogCreate.REQ" to create the data log file (csv) on the webserver. Then ckeck if the data log file (csv) exists on the webserver by typing the IP address in your browser. The application (http://support.automation.siemens.com/WW/view/en/64396156) works. I upgrated it to V13 and updated the CPU to V3. Perhaps you have to delete the csv files on your webserver by resetting the CPU via "Online & diagnostics > Functions > Reset the CPU to factory settings" and download the project again. |
3/23/2017 4:02 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4773 Rating: (123) |
New question published by Manuprasad is split to a separate thread with the subject continuously record selected variables. Best regards |
Follow us on