10/14/2015 8:21 PM | |
Posts: 8 Rating: (0) |
HI So........ I have a lot of questions, i am still on baby steps regarding all this and I know i have lots to learn, so i hope some of you guys can help me with some of this questions, which some of you may find to be very basic ones So.....first of all *******I'm using a SINAMICS S110 CU305PN with a S7-315-2PN/DP connected via PROFINET trying to control a siemens servo and i will have to also control a SEW induction motor with an encoder******* 1.- What is a Telegram? What does PZD means and the numbers "x/y" ; eg "Free Telegram PZD-16/16?? What's the difference between all of them (telegrams), and which one should I use?
And it uses Telegram 111 to communicate, first i configured it in HW Config, and then when configuring in Starter, it says (page 48) that i should [ "In the screen form "Process data exchange", select the "PROFIdrive telegram"as the setpoint source, and "[111] SIEMENS telegram 111, PZD-12/12" as telegram type. ] But no SIEMENS telegram 111, PZD-12/12 appears Something like this was mentioned in this thread: And in the imgs attached by "miami" user he shows where both telegrams have to be configured and be the same, in HW Config and Starter, but when i try to configure Telegram 111 in Starter, i dont get the options to choose Telegram 111 i get other telegrams to choose. Pics attached. So.... should it always be Telegram 111 when using a S110 or.......can other Telegrams be used??????
I can already get a connection via connect target ( i was having problems with that, like i mentioned in this thread i made : https://support.industry.siemens.com/tf/ww/en/posts/sinamics-s110-cu305pn- connections-problems-with-315-2pn-cpu/135167/?page=0&pageSize=10) but know when i try to assume control in the Commisioning-->Control Panel just like this video in 0:52 to 1:06 https://www.youtube.com/watch?v=KIkLAT6Qt5w i get an error, "The switch-on disable of the drive is active". img attached. And when i check the alarms tab and click it, it sends me to help and it mentions cause/remedy (img attached) and it says
3. At this moment I'm using SIMATIC MANAGER v5.5+sp3, STARTER V4.4.0.3 but i also have TIA PORTAL V13 SP1 Update 5 so my other question can i configure and use the S110 directly in TIA Portal, someone told me that you could only use the G series in tia portal via startdrive, that the S series couldn't be done in TIA; that i should use STARTER and SIMATIC to get it done; is this so?? because i just found this
--at pg.13 it says i should change the "Optimized BLock Access" attribute to a DB, but it doesn't let me check or uncheck when i try to do it, why would this be??? --at pg.16 it says "The configuration of SINAMICS G120/S120 will be not described in this which configuration do they mean, the one in STARTER, should it be done in STARTER first????? no startdrive or other program or what??? 4. I almost forgot to mention that when i go to "Connect target device" a message appears telling me that the target device gsd_files_v04_30_13_00 and SINAMICS_S110 software_V4_4_SP3 and im using starter Product: Drive ES - Starter is there an update i am missing or someother files??????? SORRY FOR SUCH A LONG POST and this beginner questions, im still a student but i really want to learn how to do this and as of know i need help, there is only 1 guy at work that knows a bit about this but when asked him he didn't know and he is the only 1 that knows about SINAMICS i really hope you guys can help me :| THANKS IN ADVANCE Attachmentimages.rar (172 Downloads) |
Follow us on