11/27/2010 11:22 PM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Hello f.arslan, 1st of all you can go in hardware configuration and under the options menu, you will find install hardware updates just above install GSD file. Click it and mark download from internet then Execute. download the new products that you need (or download them all) then close and don't forget to Install what you have downloaded. If it's not working with you this way then you can download the GSD file directly from this link, PROFIBUS GSD files : ET 200M. Best regards, H-H |
11/28/2010 11:05 AM | |||||||
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359) |
Dear f.arslan check the version of your STEP7, more detail on : New IM153-2 with New Functions Released for Delivery.
regards |
||||||
Last edited by: hdhosseini at: 11/28/2010 11:12 AM |
|||||||
This contribution was helpful to1 thankful Users |
12/2/2010 3:07 PM | |
Joined: 9/27/2006 Last visit: 5/7/2024 Posts: 12257 Rating: (2666) |
Hello f.Arslan; Where have you selected the IM-153-2 in your catalog? Have you opened the DP/PA Link section of the Profibus slaves? This is where you will find the model of IM-153-2 that you can use as an interface between DP and PA networks. Look at the following manual on DP/PA links, couplers and Y-Links; study the setup example you will find in the Commissioning the DP/PA Link chapter: http://support.automation.siemens.com/WW/view/en/1142696 Hope this helps, Daniel Chartier |
11/3/2017 9:55 AM | |
Joined: 6/19/2017 Last visit: 5/7/2024 Posts: 8002 Rating: (163) |
New question published by ihsei908 is split to a separate thread with the subject How can download or upgrade the simatic s7 v5.5?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on