11/29/2019 10:28 AM | |
Joined: 10/11/2006 Last visit: 4/24/2024 Posts: 5823 Rating: (789)
|
Hello, are you planning to use the SIMATIC library LCon to control the two winders or are you planning to run it in the drive? A description of all winder applications can be found under the following link: https://support.industry.siemens.com/cs/de/en/view/109744606 For SIMATIC it depends on your control mode (torque or speed controlled) and the type of controller (S7-1200 without technology objects / S7-1500 using technology objects). A description of the different solutions for SIMATIC can be found under the following link: |
With best regards, |
|
Follow us on