7/15/2019 2:08 AM | |
Posts: 2 Rating: (0) |
Hello, Would you mind to share the updated project to V15? That would be very helpful! |
10/8/2019 8:19 AM | |
Posts: 8 Rating: (1) |
Alternatively, you could also use SQL4automation. It works very well with almost all Siemens S7 PLCs. The FBs are for TIA and Step 7 Classic. All databases with ODBC connector are supported. The demo version you can download here: https://www.sql4automation.com/en/license-models/download.php The tutorial you can watch here: https://www.sql4automation.com/en/video-tutorial/2019/10/Tutorial_T006.php
|
1/27/2023 10:30 AM | |
Joined: 5/23/2019 Last visit: 9/24/2024 Posts: 90 Rating: (2) |
If you are into making your own C# (or VB) program, you could use the github project (or nuget) of S7Net+, which allows you to communicate with any siemens PLC efficiently (<10ms per read/write). S7NetPlus/s7netplus: S7.NET+ -- A .NET library to connect to Siemens Step7 devices (github.com) |
Follow us on