3/10/2018 9:45 AM | |
Joined: 5/23/2017 Last visit: 11/19/2018 Posts: 10 Rating: (0) |
There I had upload screens of Online&Diagnostic from HMI_1 to check if sth is wrong: --Deleted Link-- The only one thing made me think that is if I change the MAC adress of the device it will be replaced by zeros after any action, even switching subcard to different one and going back to this one. About other version of project: the only difference is ticked "use router" but I have checked without it and the problem still exist. Attachmentimages.zip (521 Downloads) |
Last edited by: Jen_Moderator at: 3/12/2018 10:54:43 AMDeleted link and added all files as an attachment. |
|
12/19/2018 4:44 PM | |
Joined: 1/2/2017 Last visit: 7/11/2023 Posts: 284 Rating: (23) |
Hello I had the same problem today, it happened after I change the "Style of the HMI device" in the Runtime settings to Fresh. the problem solved by putting it back to as it was. so I guess you made some change in your project in the run time settings and now even if you do a new project , it still has the same old settings . my suggestion is to put everything to the default and see what you will get. Regards T_Ebrahem |
Disclaimer: While I strive to ensure that the content of posts and answers is accurate and complete, my posts and answers are provided “as is” and “as available.” Your use of my posts and answers content is entirely at your own risk. |
|
1/29/2020 8:01 PM | |
Joined: 5/4/2018 Last visit: 4/22/2024 Posts: 3 Rating: (0) |
I have the same issue. Did you find a solution? A long time ago so I am not hopeful.. |
2/24/2020 8:41 AM | |
Joined: 1/23/2017 Last visit: 1/8/2024 Posts: 7 Rating: (0) |
Sombody heve solve this Problem? I have the same problem with Tp1200 Comfort |
Follow us on