10/22/2020 10:52 AM | |
Joined: 10/30/2019 Last visit: 9/3/2024 Posts: 7 Rating: (0) |
Good morning Christoph I have the same problem i used TIA Portal V15 to upload the program, but i couldn't cuz i got message that the blocks can only be edited with Step 7 V11 SP2, so i downloaded V11 SP2 but unfortuanlty i didn't find my CPU part number in the library of the CPUS Now my question: How can i add my Cpu to the library or what can i should do ? Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/22/2020 13:39:04New subject after splitting |
|
10/22/2020 11:23 AM | |
Joined: 3/30/2020 Last visit: 9/20/2024 Posts: 4777 Rating: (981) |
Hello. The description misses important information like which CPU you are trying to reach. Also no mention if you have loaded all updates for the software. 95% chance that you find what you are looking for here... |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
10/22/2020 12:29 PM | |
Joined: 10/30/2019 Last visit: 9/3/2024 Posts: 7 Rating: (0) |
Hello Thanks for your reply Actually my CPU part number that i want to reach is ( Dc/Dc/Rly 6ES7 212-1HE31-0XB0 ) and the only CPU part number that i can see on V11 SP2 is ( Dc/Dc/Rly 6ES7 212-1HD30-0XB0 ) I downloaded the ( HSP ) of V11 SP that i found on your attached link and then installed it but also didn't find my part number Cpu Any Recommendation ? |
10/22/2020 1:13 PM | |
Joined: 3/30/2020 Last visit: 9/20/2024 Posts: 4777 Rating: (981) |
The PDF that is listed with the HSP for Step7 V11 The PDF also states that at least Step7 V11 SP2 Update 3 is needed. I recommend you read documentations on how to update the HSP if you have difficulty using the HSP. Good luck. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
Follow us on