11/5/2020 4:22 PM | |
Posts: 9 Rating: (0) |
The belt is now actually moving about 2mph in this picture. |
11/6/2020 5:29 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
The attachment shows how part of the logic works and it is based on a drive set for a max frequency of 114.80 Hz. I can not recommend making any changes to the drive parameters, commissioning the drive for the motor connected to it and the application is your responsibility. Reboot the entire system by turning the power off and wait a couple of minutes then turn it back on. There are two inputs that must be ON, The E-STOP I0.0 and Exercise Machine Switch I1.0 Do not press any buttons or make change settings on the HMI other than the buttons you showed in the images you uploaded, specifically there may be a button "Change speed" on some screen somewhere, do not press it. Press STOP button on HMI, just to be sure. Then press forward or reverse button and then start increasing the speed; that should work just like that, if it doesn't then you will need to provide much much more information: - Image of motor plate -Communication parameters set in drive. -Motor parameters set in drive. Attachmenttreadmill.zip (189 Downloads) |
Follow us on