8/13/2010 5:08 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684)
|
Hello 256; With this type of question, I can only really suggest you take a few minutes and study the Programming with Step 7, v. 5.4 reference manual: http://support.automation.siemens.com/WW/view/en/18652056 Chapter 19 is dedicated to downloading amnd uploading procedures. Chapter 24 presents printing and archiving with Step 7. There is also the online help of Step 7 that can be immensely helpful for information on the different options in the Step 7 editors. Hint: if you need to print a program inladder, go to the program editor, view your program in LAD, and look for the File --¨Print menu... Hope this helps, Daniel Chartier |
This contribution was helpful to3 thankful Users |
4/25/2012 2:43 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, Follow the attached Pdf. My CPU is a simulated one, so it looks a bit different. Note thatin your uploaded program there are no symbols, variable names and comments. Succes, Regards, Marcjan Attachmentupload.pdf (7139 Downloads) |
Last edited by: Marcjan at: 4/25/2012 2:44 PMProblem solved? |
|
This contribution was helpful to11 thankful Users |
7/11/2013 2:49 PM | |
Posts: 13 Rating: (0) |
hi hdhosseini Can u explain that Downloading proceedure in detail, Iam expectingclear proceedure .. thnaks, vadi |
7/11/2013 3:23 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hi vadi, You know the place connector for the CPU and the MPI address? |
7/11/2013 3:25 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello Mothilal, Same question of vadi: You know the place for the CPU connector and the MPI address? |
Follow us on