11/5/2020 5:04 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197)
|
Download for LOGO! 8.3 Software UpgradeDownload and installation instructions for the LOGO! Soft Comfort Upgrade to the Version V8.3. The upgrade contains:
Installation instructions for the LOGO! Soft Comfort Upgrade to the Version V8.3: The predecessor version of LOGO! Soft Comfort on PC is required for installation. Alternatively, you can also use an existing LOGO! Soft Comfort DVD during the installation. What's new with LOGO! Soft Comfort V8.3:
The order number for LOGO! Soft Comfort remains unchanged. The stock at EC will be sold out. Note: A DAMEX check is required to download the free upgrade to SIOS (FAQ: Support ID109744535) What's new with LOGO! Web Editor Version V1.1:
Note: A DAMEX check is required to download the Web Editor V1.1. (FAQ: Support ID109744535) |
Last edited by: ixo65 at: 01/09/2021 03:37:04 |
|
This contribution was helpful to5 thankful Users |
1/27/2021 7:21 PM | |
Posts: 1 Rating: (0) |
how long that damex check should take?? i have waiting 4 days now and my customer waits program to new logo.... i cant send program v.8.2 to that new logo. |
1/27/2021 7:24 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197)
|
Nobody in this user forum can give you a correct answer, only Siemens. Other users wait up to 14 days .... |
2/4/2021 1:22 PM | |
Joined: 8/3/2017 Last visit: 6/11/2024 Posts: 1086 Rating: (53) |
Hi RossHall, I understand your disappointment - but you have to see it from the other side: if the software is accessible for everyone than there could be bad consequences, too. It is not for nothing that there are laws that require export approval: https://support.industry.siemens.com/cs/de/en/view/109744535 And as ixo65 already said.. when someone willing to download the software from a not official webpage than he agress to do somethin illegal.. |
Please, check out the forum search to find already existing topics regarding your issue and to get some hints. |
|
2/5/2021 2:22 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197)
|
Unfortunately nobody can tell you that here in the forum ... |
Follow us on