11/27/2007 10:51 AM | |
Joined: 10/3/2006 Last visit: 1/5/2024 Posts: 44 Rating: (0) |
Hi, I have a working PCS7 v6.1 system consisting of 1 OS Server, 1 OS Standby, 3 OS Clients (1 acting as a Web Server), and 1 Central Archive Server. I have made a picture in WinCC that monitors the life beat of all the PCs which is working fine. But as seen on the Web Server, the life beat monitor for the Central Archive Server is not working. I have attached graphics files to have a clear view of the problem. Even after several compilation of Web Navigator and a couple of restarts the problem still persists. What should I do to fix this? Attachmentwincc and web snapshots.zip (277 Downloads) |
12/10/2007 2:35 AM | |
Joined: 10/3/2006 Last visit: 1/5/2024 Posts: 44 Rating: (0) |
Hi Mr. Mario, Thanks.I will try this today. I will give you feedback later. Regards, Jenie |
Follow us on