(3)| 2/9/2012 10:12 AM | |
|
Posts: 2 Rating:
|
Works perfect. Thanks |
| 3/1/2012 4:25 PM | |
|
Posts: 7 Rating:
|
Get rid of the TCON command, you don't need it. I don't have it in my code and it is not required. |
| 3/1/2012 11:54 PM | |
|
Joined: 3/11/2007 Last visit: 6/6/2025 Posts: 226 Rating:
|
Here is available for download an example of sending email. Hello /tf/WW/en/Posts/67185#top |
This contribution was helpful to
|
|
| 10/31/2012 9:52 AM | |
|
Joined: 3/2/2012 Last visit: 5/15/2025 Posts: 1 Rating:
|
Does someone have a working example? i've bin trying to get the TM_MAIL working, i do not see what i'm doing wrong. |
| 10/31/2012 2:51 PM | |
|
Joined: 7/7/2010 Last visit: 12/19/2025 Posts: 16321 Rating:
|
Look up just a couple of posts to the one by automatizzando. Follow their link to just near the end and find their posted example. |
|
science guy |
|
| 1/31/2013 2:40 PM | |
|
Joined: 10/22/2008 Last visit: 12/9/2025 Posts: 378 Rating:
|
What I would like to add to the post is that I tried TM_MAIL few days ago and works ok. - smtp server with 25 port open - 1214 -1hg31- FW 3.0.2 - TM_MAIL v 1.1 - TIA v11 SP2 UP5 P.S. The eWONdevices looks very nice. Is it really so easy to use? Is it the sameas VIPA devices? |
| 1/31/2013 5:55 PM | |
|
Posts: 7 Rating:
|
As a Siemens distributor here in the U.S., I probably can't discuss Ewon devices in their forums. All I can say is, YES, they are VERY easy to use, and I have many customers using them to access their Siemens-based systems all around the world. I have no idea if they make them for VIPA or not. Frankly, I was hoping Siemens would simply "buy" Ewon and market them as Siemens products because they work so well with Siemens products via ethernet OR Profibus. ;) I also wish Siemens would some day allow us to modify the Port 25 address. I know somebody stated in this thread that it can be modified, but I don't believe that to be true at all. Good luck! |
Follow us on