(0)| 10/24/2013 2:50 PM | |
|
Posts: 4620 Rating:
|
Hi tcangar, Another thinking, the motor is connected to the load? If yes you can try to disconnect the load and see if the message still appears. |
| 10/24/2013 3:54 PM | |
|
Posts: 4620 Rating:
|
Hi, Have you tried to run themotor alone? Without load? What happens? |
| 10/24/2013 4:19 PM | |
|
Posts: 20 Rating:
|
I have to mechanically dismount the motor shaft, pulleys and other stuff, which is not a simple thing to begin with. |
| 11/5/2013 9:11 AM | |
|
Posts: 20 Rating:
|
Thanks Vithani. I made the Quick-Setup once more, it's working now fine, maybe I made an error in the internal motor parameters or the Quick Setup procedure was not closed properly. [schnippschnapp] New question was splitted to is it possible to set the parameter P0640 to 50%? |
Last edited by: O_Moderator at: 11/6/2013 8:57 AM |
|
This contribution was helpful to
|
|
| 8/28/2014 12:36 PM | |
|
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
New question was split to When i start the drive without load just with the motor it shows alarm A0501. Best regards O_Moderator |
Follow us on