6/14/2020 12:42 AM | |
Posts: 42 Rating: (1) |
Hi guys. I have the same problem. The ip of my logo is 192.168.1.38 and for this ip i have opened the port 8080. My public ip is for exemple xx.xx.xx.xx When i search on the internet xx.xx.xx.xx:8080 i cannot connect. What am i doing wrong? I'm looking forward to hearing from you. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/15/2020 09:00:40New subject after splitting |
|
6/14/2020 4:33 PM | |
Posts: 42 Rating: (1) |
Okey, i will try it later. The ip of the image is your LOGO! Ip? Thanks for your help? |
6/14/2020 4:35 PM | |
Joined: 12/18/2014 Last visit: 9/25/2024 Posts: 33837 Rating: (4205)
|
Yes, it's the IP address of one of LOGO!s. |
6/15/2020 12:57 PM | |
Posts: 42 Rating: (1) |
Hi ixo65. I think that did port forwarding and it doesn`t work yet. In the zip i've appended two screenshots, have a look if you want. One with the forwarding setup and how it works with my subnet through 8080 port. The second picture is a screen of my phone, it doen't work using my public ip and 8030 port (the forwarded port). Is very strange. Regards. AttachmentSiemens_Forum.zip (119 Downloads) |
Last edited by: Berguinsson at: 06/15/2020 12:57:47 |
|
6/15/2020 9:04 PM | |
Posts: 40 Rating: (0) |
Forget about LOGO! for a while. Configure port forwarding for the IP of your PC and run Wireshark there. Then try to make a connection from outside. |
Follow us on