6/2/2009 5:45 PM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Hi saravana kumar AttachmentY-Link.zip (293 Downloads) |
Best Regards |
|
This contribution was helpful to1 thankful Users |
6/3/2009 5:43 AM | |
Joined: 2/6/2009 Last visit: 3/21/2024 Posts: 938 Rating: (118) |
Hi Khaled_Ezzat , Thank you for your reply. The picture you have sent is showing about the one H-System bundle,But My question is, If there is another H-System Bundle similar to the first onemeanshow to communicate between those H-Systems through profibus. |
_______________________________________________________________ |
|
6/3/2009 6:19 AM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665)
|
Hello kumar; A Y-Link is an interface between a redundant Profibus master (on a S7-400H system) and single-line Profibus slaves. As such, you can setup a S7-300 or S7-200 CPU, for example, as a slave to a S7-400H using a Y-link, as well as any standard DP slave. However, in a S7-400H system, the S7-400 cannot be setup as a slave. This is specified in the S7-400H system manual, discussing the limitations of S7-400 CPUs when used in a redundant system: http://support.automation.siemens.com/WW/view/en/1186523 The manual also contains a chapter on recommended networks forpairs ofS7-400H systems, over Industrial Ethernet or using Profibus-DP (with2 CP 443-5 Extended) Alternatively, you could examine the possibility of using a DP/DP coupler between 2 Y-Links (one on each S7-400H system). I have never done this myself, I have heard this possibility discussed by collegues, but maybe someone here on the forum could seeif it could be done. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/3/2009 6:20 AM |
|
This contribution was helpful to1 thankful Users |
6/3/2009 1:09 PM | |
Posts: 557 Rating: (64) |
hi yes it is possible, by using a dp dp coupler,we can communicate between two H system by using Y LINK.......... REGARDS |
6/3/2009 3:28 PM | |
Joined: 2/6/2009 Last visit: 3/21/2024 Posts: 938 Rating: (118) |
Hi Eastern,dchartier,Khaled_Ezzat , Thank you for your help.Now got one solution. I am going totry by usingSFC65 X_SEND & SFC66 X_RCV(PROFIBUS master-master connection). |
Last edited by: saravana kumar at: 6/3/2009 3:30 PM_______________________________________________________________ |
|
This contribution was helpful to1 thankful Users |
Follow us on