10/8/2015 5:24 PM | |
Posts: 111 Rating: (1) |
I NEED 24VDC REMOTE I/OS WITH 16 INPUT AND 16 OUTPUT I AM HAVING A PROBLEM IN UNDERSTANDING WHICH ONE I SHOULD USE E200SP AND E200MP. WHAT IS THE DIFFERENCE BETWEEN BOTH OF THEM. MY APPLICATION IS I NEED TO TURN MOTORS ON AND ACTIVATE VALVES THROUGH OUTPUTS AND NEED INPUT FOR SENSORS. CAN ANYBODY HELP? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/9/2015 9:24:20 AMNew subject after splitting |
|
10/9/2015 8:41 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi, ET200SP is smaller than ET200MP. It is another kind of remote I/O´s. ET200MP Interfacemodules are handling with the electronic-modules of S7-1500-series. To see the general differences have a look in the system manuals: SIMATIC ET 200SP Distributed I/O systemSIMATIC S7-1500, ET 200MP Automation systemhope this helps, regards, |
FCK WAR! |
|
10/14/2015 1:53 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
Hi, and which number you have use?
Christoph |
Last edited by: ChristophD at: 10/14/2015 2:01:21 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on