7/2/2010 3:52 PM | |
Posts: 7 Rating: (0) |
i have atlas copco compressor with inverter micromaster 440 built in, now the inverter broke down and i would like to replace with sinamics, then the compressor controller's (Elektronikon II) could not communicate with the inverter (sinamics) with rs485 connection, the message is "Converter Format Failure'. The Atlas Copco man said that the controller could only communicat with micromaster 440. The different parameter between Sinamics and Micromaster is memory R0203 that indentify the inverter type (2 for micromaster). Anyone can help me solve the problem? Regards, Iman HG Jakarta Indonesia Splitted from simovert vc of Atlas copco compressor. |
Last edited by: O_Moderator at: 7/5/2010 9:32 AMnew subject after splitting |
|
8/14/2017 12:20 PM | |
Joined: 6/19/2017 Last visit: 5/10/2024 Posts: 8026 Rating: (163) |
New question published by gaz2010 is split to a separate thread with the subject Since GA50CSD came back from repair it will not communicate with the elekronikon ii and keep receiving the converter timeout message. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on